DOCA0193EN-00

Miscellaneous

Nominal Current

Address

Register

RW

X

Unit

Type

Range

Description

0x222D

8750

R

1

A

INT16U

0–8000

Rated circuit breaker current
Factory setting = 100 A (circuit breaker sensor plug not present)

Battery Status

Address

Register

RW

X

Unit

Type

Range

Description

0x228A

8843

R

1

%

INT16U

0–100

Battery-charge indicator:
100 % = U > 2800 mV
50 % = 2200 < U < 2800 mV
0 % = U < 2200 mV

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.