DOCA0193EN-00

List of IO Module Commands

List of Commands

There are two types of command:

  • generic commands, which work independently of the application selected.

  • application commands, which are dedicated to an application. A command is only valid if the related application is configured.

The following table lists the available IO module commands, their corresponding application, command codes and user profiles. Follow the command execution procedures accordingly. (refer to Executing a Command).

Application

Command

Command code

User profile

Generic

Change output state (refer to Change Output State)

1672

Administrator or Operator

Generic

Reset IO module alarms (refer to Reset IO Module Alarm)

41099

Administrator or Operator

Generic

Enable/Disable simple commands (refer to Enable/Disable Simple Commands)

41100

Administrator or Operator

Generic

Acknowledge latched output (refer to Acknowledge Latched Output)

41102

Administrator or Operator

Generic

Reset analog input minimum/maximum values (refer to Reset Analog Input Minimum/Maximum Values)

42890

Administrator or Operator

Cradle management

Preset cradle counters (refer to Preset Cradle Counters)

41352

Administrator or Operator

Cradle management

Preset cradle regrease timers (refer to Preset Regrease Timers)

41353

Administrator or Operator

Light control

Light control (refer to Light Control)

42120

Administrator or Operator

Load control

Load control (refer to Load Control)

42376

Administrator or Operator

Pulse counter management

Preset input pulse counter (refer to Preset Input Pulse Counters)

42888

Administrator or Operator

Cooling system

Preset switchboard temperature threshold counter (refer to Preset Switchboard Temperature Threshold Counters)

42889

Administrator or Operator

IO Module Error Codes

The error codes generated by the IO module are the generic error codes (refer to Result of the Command).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.