DOCA0193EN-00

About the Book

Document Scope

The aim of this document is to provide users, installers, and maintenance personnel with the technical information needed to operate the Modbus protocol on the EasyPact MVS circuit breakers.

Validity Note

This document is valid for EasyPact MVS circuit breakers with a BCM ULP circuit breaker communication module embedded. It is connected to an RS 485 serial line Modbus network using an IFM Modbus-SL interface for one circuit breaker.

This document describes the registers and commands available for the IMU modules with the following firmware version:

To Do: Firmware version to be updated for ETV trip system in the next release.

IMU Module

Part Number

Firmware Version

ETV trip system

BCM ULP module

33106

≥ V4.1.9

IO module

LV434063

≥ V003.004.005

IFM interface

LV434000

≥ V003.001.012

Online Information

The information contained in this guide is likely to be updated at any time. Schneider Electric strongly recommends that you have the most recent and up-to-date version available on www.se.com/ww/en/download.

The technical characteristics of the devices described in this guide also appear online. To access the information online, go to the Schneider Electric home page at www.se.com.

Related Documents

Title of Documentation

Reference Number

EasyPact MVS Circuit Breakers – User Guide

MVS21734

IO Input/Output Application Module for One Circuit Breaker – User Guide

DOCA0055EN

ULP (Universal Logic Plug) System – User Guide

DOCA0093EN

EasyPact MVS – Installation Manual

MVS21735

EasyPact MVS Circuit Breaker Accessories – Installation Manual

MVS21736

EasyPact MVS Chassis Accessories – Installation Manual

MVS21737

EasyPact MVS – Interlocking of EasyPact MVS Devices – Installation Manual

MVS21738

Input/Output Application Module for One Circuit Breaker – Instruction Sheet

HRB49217

IFM - Modbus-SL Interface for One Circuit Breaker – Instruction Sheet

NVE85393

EasyPact MVS – Catalog

LVED211021EN

You can download these technical publications and other technical information from our website at https://www.se.com/en/download.

Trademark Notice

All trademarks are owned by Schneider Electric Industries SAS or its affiliated companies.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.