DOCA0193EN-00

BCM ULP Module Identification

Product Identification

Address

Register

RW

X

Unit

Type

Range

Description

0x0202

515

R

INT16U

15139

Product identification = 15139 for the BCM ULP module

BCM ULP Module Identifier

Address

Register

RW

X

Unit

Type

Range

Description

0x0215–0x0216

534–535

RW

OCTET STRING

0x0000–0x7F7F

Short identifier of BCM ULP module coded over 4 ASCII characters
Factory setting = 0x0000

0x0217–0x021E

536–543

RW

OCTET STRING

0x0000–0x7F7F

Long identifier of BCM ULP module coded over 16 ASCII characters
Factory setting = 0x0000

BCM ULP Module Firmware Version

The BCM ULP module firmware version starts with a V character and has the following format: VX.Y.Z.

The firmware version is coded as follows: VX.Y.Z = VX*1000 + Y*100 + Z*10

For example if the value of the register is equal to 2000, the BCM ULP module firmware version is equal to V2.0.0.

Address

Register

RW

X

Unit

Type

Range

Description

0x0240

577

R

INT16U

BCM ULP module firmware version

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.