DOCA0193EN-00

Maintenance Indicators

Load Profile Counters

The load profile counters report the number of hours for each range of current in the ETV trip system. If the load profile counters reach the maximum value
4 294 967 295 and a new load profile event occurs, then the load profile counters are reset to 0.

A read request of eight registers is necessary to read the load profile counters.

Address

Register

RW

X

Unit

Type

Range

Description

0x74B7–0x74B8

29880–29881

R

1

Hour

INT32U

0–4 294 967 295

Number of hours for 0–49% of the nominal current range

0x74B9–0x74BA

29882–29883

R

1

Hour

INT32U

0–4 294 967 295

Number of hours for 50–79% of the nominal current range

0x74BB–0x74BC

29884–29885

R

1

Hour

INT32U

0–4 294 967 295

Number of hours for 80–89% of the nominal current range

0x74BD–0x74BE

29886–29887

R

1

Hour

INT32U

0–4 294 967 295

Number of hours for 90–100% of the nominal current range

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.