DOCA0193EN-00

Standard Dataset Common Registers

Circuit Breaker Status Register

Address

Register

RW

Unit

Type

Range

Bit

Description

0x7CFF

32000

R

INT16U

Quality of each bit of register 32001 (refer to Quality of Bits in Registers):

  • 0 = Invalid

  • 1 = Valid

0x7D00

32001

R

INT16U

Circuit breaker status register

0

OF status indication contact

  • 0 = The circuit breaker is open.

  • 1 = The circuit breaker is closed.

1

SD trip indication contact

  • 0 = Circuit breaker is not tripped.

  • 1 = Circuit breaker is tripped due to electrical fault, shunt trip, or push-to-trip.

Bit always equal to 0 for EasyPact MVS circuit breakers with motor mechanism.

2

SDE fault trip indication contact

  • 0 = Circuit breaker is not tripped on electrical fault.

  • 1 = Circuit breaker is tripped due to electrical fault (including ground-fault test).

3

CH spring charged contact

  • 0 = Spring discharged

  • 1 = Spring charged

Bit always equal to 0 for EasyPact MVS circuit breakers with motor mechanism.

4

Reserved

5

PF ready to close contact

  • 0 = Not ready to close

  • 1 = Ready to close

Bit always equal to 0 for EasyPact MVS circuit breakers with motor mechanism.

6–14

Reserved

15

Data availability

If this bit is set at 1, all other bits of the register are not significant.

IO Status Registers

Address

Register

RW

Unit

Type

Range

Bit

Description

0x7D01

32002

R

INT16U

Quality of each bit of register 32003 (refer to Quality of Bits in Registers):

  • 0 = Invalid

  • 1 = Valid

0x7D02

32003

R

INT16U

IO1 module and M2C status

0

Digital input 1 status:

  • 0 = Off

  • 1 = On

1

Digital input 2 status:

  • 0 = Off

  • 1 = On

2

Digital input 3 status:

  • 0 = Off

  • 1 = On

3

Digital input 4 status:

  • 0 = Off

  • 1 = On

4

Digital input 5 status:

  • 0 = Off

  • 1 = On

5

Digital input 6 status:

  • 0 = Off

  • 1 = On

6

Digital output 1 status:

  • 0 = Off

  • 1 = On

7

Digital output 2 status:

  • 0 = Off

  • 1 = On

8

Digital output 3 status:

  • 0 = Off

  • 1 = On

9

Digital M2C output 1 status:

  • 0 = Off

  • 1 = On

10

Digital M2C output 2 status:

  • 0 = Off

  • 1 = On

11–14

Reserved

15

Data availability

If this bit is set at 1, all other bits of the register are not significant.

0x7D03

32004

R

INT16U

Quality of each bit of register 32005:

  • 0 = Invalid

  • 1 = Valid

0x7D04

32005

R

INT16U

IO2 module status

0

Digital input 1 status:

  • 0 = Off

  • 1 = On

1

Digital input 2 status:

  • 0 = Off

  • 1 = On

2

Digital input 3 status:

  • 0 = Off

  • 1 = On

3

Digital input 4 status:

  • 0 = Off

  • 1 = On

4

Digital input 5 status:

  • 0 = Off

  • 1 = On

5

Digital input 6 status:

  • 0 = Off

  • 1 = On

6

Digital output 1 status:

  • 0 = Off

  • 1 = On

7

Digital output 2 status:

  • 0 = Off

  • 1 = On

8

Digital output 3 status:

  • 0 = Off

  • 1 = On

9–14

Reserved

15

Data availability

If this bit is set at 1, all other bits of the register are not significant.

Tripping Cause

The tripping cause register provides information about the cause of the trip for the standard protection functions. When a tripping cause bit is at 1 in the tripping cause register, it indicates that a trip has occurred and has not been reset.

The tripping cause bit is reset as soon as the circuit breaker is closed again.

Address

Register

RW

Unit

Type

Range

Bit

Description

0x7D05

32006

R

INT16U

Quality of each bit of register 32007 (refer to Quality of Bits in Registers):

  • 0 = Invalid

  • 1 = Valid

0x7D06

32007

R

INT16U

Tripping cause for the standard protection functions

0

Long-time protection Ir

1

Short-time protection Isd

2

Instantaneous protection Ii

3

Ground-fault protection Ig

4

Reserved

5

Integrated instantaneous protection (SELLIM and DIN/DINF)

6

Other protections

7

Internal failure (overvoltage)

8–14

Reserved

15

If this bit is at 1, bits 0 to 14 are not valid.

0x7D07–0x7D1A

32008–32027

Reserved

Current

Address

Register

RW

Unit

Type

Range

Description

0x7D1B–0x7D1C

32028–32029

R

A

FLOAT32

RMS current on phase 1

0x7D1D–0x7D1E

32030–32031

R

A

FLOAT32

RMS current on phase 2

0x7D1F–0x7D20

32032–32033

R

A

FLOAT32

RMS current on phase 3

0x7D21–0x7D22

32034–32035

R

A

FLOAT32

RMS current on the neutral(1)

0x7D23– x7D24

32036–32037

R

A

FLOAT32

Maximum of RMS current of phases 1, 2, 3 and N (most loaded phase)(2)

0x7D25–0x7D26

32038–32039

R

FLOAT32

Current ratio on ground (Ig setting ratio)

(1) Value available when system type register returns 30 or 41.

(2) Value reset: see the reset minimum/maximum command.

Maximum Current Values

Maximum current values can be reset with the reset minimum/maximum command.

Address

Register

RW

Unit

Type

Range

Description

0x7D29–0x7D2A

32042–32043

R

A

FLOAT32

Maximum RMS current on phase 1

0x7D2B–0x7D2C

32044–32045

R

A

FLOAT32

Maximum RMS current on phase 2

0x7D2D–0x7D2E

32046–32047

R

A

FLOAT32

Maximum RMS current on phase 3

0x7D2F–0x7D30

32048–32049

R

A

FLOAT32

Maximum RMS current on the neutral(1)

0x7D31–0x7D32

32050–32051

R

A

FLOAT32

This is the highest (i.e. maximum) maximum current value since this measurement was last reset. The measurement looks at all 3 currents, MaxI1, MaxI2, MaxI3, and MaxIN, and keeps track of the highest value of any of them over time.

(1) Value available when system type register returns 30 or 41.

Voltage

Address

Register

RW

Unit

Type

Range

Description

0x7D37–0x7D38

32056–32057

R

V

FLOAT32

41.6–2250

RMS phase-to-phase voltage V12

0x7D39–0x7D3A

32058–32059

R

V

FLOAT32

41.6–2250

RMS phase-to-phase voltage V23

0x7D3B–0x7D3C

32060–32061

R

V

FLOAT32

41.6–2250

RMS phase-to-phase voltage V31

0x7D3D–0x7D3E

32062–32063

R

V

FLOAT32

24-1500

RMS phase-to-neutral voltage V1N(1)

0x7D3F–0x7D40

32064–32065

R

V

FLOAT32

24-1500

RMS phase-to-neutral voltage V2N(1)

0x7D41–0x7D42

32066–32067

R

V

FLOAT32

24-1500

RMS phase-to-neutral voltage V3N(1)

(1) Value available when system type register returns 40 or 41.

Power

Address

Register

RW

Unit

Type

Range

Description

0x7D47–0x7D48

32072–32073

R

W

FLOAT32

-16000000–16000000

Active power on phase 1(1) (2)

0x7D49–0x7D4A

32074–32075

R

W

FLOAT32

-16000000–16000000

Active power on phase 2(1) (2)

0x7D4B–0x7D4C

32076–32077

R

W

FLOAT32

-16000000–16000000

Active power on phase 3(1) (2)

0x7D4D–0x7D4E

32078–32079

R

W

FLOAT32

-16000000–16000000

Total active power(2)

0x7D4F–

0x7D50

32080–32081

R

VAr

FLOAT32

-16000000–16000000

Reactive power on phase 1(1) (2)

0x7D51–0x7D52

32082–32083

R

VAr

FLOAT32

-16000000–16000000

Reactive power on phase 2(1) (2)

0x7D53–0x7D54

32084–32085

R

VAr

FLOAT32

-16000000–16000000

Reactive power on phase 3(1) (2)

0x7D55–0x7D56

32086–32087

R

VAr

FLOAT32

-16000000–16000000

Total reactive power(2)

0x7D57–0x7D58

32088–32089

R

VA

FLOAT32

0–16000000

Apparent power on phase 1(1)

0x7D59–0x7D5A

32090–32091

R

VA

FLOAT32

0–16000000

Apparent power on phase 2(1)

0x7D5B–0x7D5C

32092–32093

R

VA

FLOAT32

0–16000000

Apparent power on phase 3(1)

0x7D5D–0x7D5E

32094–32095

R

VA

FLOAT32

0–16000000

Total apparent power

(1) Value available when system type register returns 40 or 41.

(2) The sign for the active and reactive power depends on the configuration of the register 3316.

Energy

Energy is stored in big-endian format: the most significant register is transmitted first.

Address

Register

RW

Unit

Type

Range

Description

0x7D5F–0x7D62

32096–32099

R

Wh

INT64

Total active energy

0x7D63–0x7D66

32100–32103

R

VARh

INT64

Total reactive energy

0x7D67–0x7D94

32104–32149

Reserved

Ground-Fault Current

Address

Register

RW

Unit

Type

Range

Description

0x7D95–0x7D96

32150–32151

R

A

FLOAT32

Ground-fault current

0x7D97–0x7D9A

32152–32155

Reserved

Current Demand Values

Address

Register

RW

Unit

Type

Range

Description

0x7D9B–0x7D9C

32156–32157

R

A

FLOAT32

Current demand value on phase 1: I1 Dmd

0x7D9D–0x7D9E

32158–32159

R

A

FLOAT32

Current demand value on phase 2: I2 Dmd

0x7D9F–0x7DA0

32160–32161

R

A

FLOAT32

Current demand value on phase 3: I3 Dmd

0x7DA1–0x7DA2

32162–32163

R

A

FLOAT32

Current demand value on the neutral: IN Dmd(1)

(1) Value available when system type register returns 30 or 41.

Power Demand Values

When the window is a fixed type, this value is updated at the end of the window. For the sliding type, the value is updated every 15 seconds.

Address

Register

RW

Unit

Type

Range

Description

0x7DA3–0x7DA4

32164–32165

R

W

FLOAT32

Total active power demand: P Dmd

0x7DA5–0x7DA6

32166–32167

R

VAR

FLOAT32

Total reactive power demand: Q Dmd

0x7DA7–0x7DA8

32168–32169

R

VA

FLOAT32

Total apparent power demand: S Dmd

0x7DA9–0x7DC0

32170–32193

Reserved

Maximum Voltage Values

Address

Register

RW

Unit

Type

Range

Description

0x7DC1–0x7DC2

32194–32195

R

V

FLOAT32

41.6–2250

Maximum RMS phase-to-phase voltage V12

0x7DC3–0x7DC4

32196–32197

R

V

FLOAT32

41.6–2250

Maximum RMS phase-to-phase voltage V23

0x7DC5–0x7DC6

32198–32199

R

V

FLOAT32

41.6–2250

Maximum RMS phase-to-phase voltage V31

0x7DC7–0x7DC8

32200–32201

R

V

FLOAT32

24–1500

Maximum RMS phase-to-neutral voltage V1N(1)

0x7DC9–0x7DCA

32202–32203

R

V

FLOAT32

24–1500

Maximum RMS phase-to-neutral voltage V2N(1)

0x7DCB–0x7DCC

32204–32205

R

V

FLOAT32

24–1500

Maximum RMS phase-to-neutral voltage V3N(1)

(1) Value available when system type register returns 40 or 41.

Power Factor

Address

Register

RW

Unit

Type

Range

Description

0x7DCD–0x7DCE

32206–32207

R

FLOAT32

Power factor on phase 1(1)

0x7DCF–0x7DD0

32208–32209

R

FLOAT32

Power factor on phase 2(1)

0x7DD1–0x7DD2

32210–32211

R

FLOAT32

Power factor on phase 3(1)

0x7DD3–0x7DD4

32212–32213

R

FLOAT32

Total power factor

0x7DD5–0x7E52

32214–32339

Reserved

(1) Value available when system type register returns 40 or 41.

Inhibit Close Order

Address

Register

RW

Unit

Type

Range

Bit

Description

0x7E53

32340

R

INT16U

Quality of each bit of register 32341:

  • 0 = Invalid

  • 1 = Valid

0x7E54

32341

R

INT16U

Inhibit close order status

0

Close breaker inhibited by IO module

  • 0 = Disable

  • 1 = Enable

1

Close breaker inhibited by communication

  • 0 = Disable

  • 1 = Enable

2–15

Reserved

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.