DOCA0193EN-00

List of IFM Interface Commands

List of Commands

The following table lists the IFM interface commands, their corresponding command codes and user profiles. Follow the command execution procedures accordingly (refer to Executing a Command).

Command

Command code

User profile

Get current time (refer to Get Current Time)

768

No password required

Set absolute time (refer to Set Absolute Time)

769

No password required

Read IMU name and location (refer to Read IMU Name and Location)

1024

No password required

Write IMU name and location (refer to Write IMU Name and Location)

1032

Administrator

Error Codes

Error codes generated by the IFM interface are the generic error codes (refer to Result of the Command).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.