DOCA0193EN-00

Hardware Setting

Addresses and Registers List

The following table describes the hardware settings addresses, and registers regarding the IO module.

IO Module

Addresses

Registers

IO 1

0x38FD–0x3902

14590–14597

IO 2

0x44B5–0x44BA

17590–17595

Hardware Setting Registers for IO 1

The order and the description of the hardware setting registers for IO 2 are the same as those of IO 1.

Address

Register

RW

Unit

Type

Range

Description

0x38FD

14590

R

INT16U

1–9

Application rotary switch current position:

  • 1 = position 1

  • 2 = position 2

  • 3 = position 3

  • 4 = position 4

  • 5 = position 5

  • 6 = position 6

  • 7 = position 7

  • 8 = position 8

  • 9 = position 9

0x38FE

14591

R

INT16U

0–1

Remote setup padlock position:

  • 0 = Unlock

  • 1 = Lock

0x38FF

14592

R

INT16U

0–1

Dip switch1 position:

  • 0 = IO 1

  • 1 = IO 2

0x3900

14593

R

Reserved

0x3901

14594

R

INT16U

1–9

Last validated application set by the test button located on the front of the IO module:

  • 1 = position 1

  • 2 = position 2

  • 3 = position 3

  • 4 = position 4

  • 5 = position 5

  • 6 = position 6

  • 7 = position 7

  • 8 = position 8

  • 9 = position 9

0x3902– 0x3904

14595– 14597

Reserved

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.