DOCA0193EN-00

Generic Commands

Change Output State

To change the output state, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

1672

Command code = 1672

0x1F40

8001

INT16U

13

Number of parameters (bytes) = 13

0x1F41

8002

INT16U

Destination =

  • IO 1: 8193 (0x2001)

  • IO 2: 8449 (0x2101)

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

Password of the command: Administrator or Operator user profile password

0x1F45

8006

INT16U

1–3

Output number:

  • 1 = output 1

  • 2 = output 2

  • 3 = output 3

0x1F46

8007

INT16U

Value to set:

  • 0x0000 = Change output state to 0 (OFF)

  • 0x0100 = Change output state to 1 (ON)

Reset IO Module Alarm

The alarms can be read from the alarm status register (refer to Alarm Status).

To reset IO module alarms, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

41099

Command code = 41099

0x1F40

8001

INT16U

10

Number of parameters (bytes) = 10

0x1F41

8002

INT16U

Destination =

  • IO 1: 8193 (0x2001)

  • IO 2: 8449 (0x2101)

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

Password of the command: Administrator or Operator user profile password

Enable/Disable Simple Commands

To enable or disable the simple commands, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

41100

Command code = 41100

0x1F40

8001

INT16U

11

Number of parameters (bytes) = 11

0x1F41

8002

INT16U

Destination =

  • IO 1: 8193 (0x2001)

  • IO 2: 8449 (0x2101)

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

Password of the command: Administrator or Operator user profile password

0x1F45

8006

INT16U

MSB: Enable or disable:

  • 0 = Disable simple command

  • 1 = Enable simple command

LSB: 0 (not used)

Acknowledge Latched Output

To acknowledge the latched output, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

41102

Command code = 41102

0x1F40

8001

INT16U

11

Number of parameters (bytes) = 11

0x1F41

8002

INT16U

Destination =

  • IO 1: 8193 (0x2001)

  • IO 2: 8449 (0x2101)

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

Password of the command: Administrator or Operator user profile password

0x1F45

8006

INT16U

MSB:

  • 0x01 = Digital output relay 1

  • 0x02 = Digital output relay 2

  • 0x03 = Digital output relay 3

  • 0xFF = Unlatch all digital output

LSB: 0 (not used)

Reset Analog Input Minimum/Maximum Values

The analog input maximum and minimum values can be read from the analog input registers (refer to Analog Input Registers of IO 1).

To reset the minimum/maximum analog input values, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

42890

Command code = 42890

0x1F40

8001

INT16U

10

Number of parameters (bytes) = 10

0x1F41

8002

INT16U

Destination =

  • IO 1: 8193 (0x2001)

  • IO 2: 8449 (0x2101)

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

Password of the command: Administrator or Operator user profile password

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.