DOCA0193EN-00

Measurement Parameters

System Type

The setup ENVT (External Neutral Voltage Tap) presence command (command code = 46472) configures the content of the system type register.

Address

Register

RW

X

Unit

Type

Range

Description

0x0CF1

3314

R-WC

INT16U

30, 31, 40, 41

System type Factory setting: 40 with ETV trip system

Determining system type:

If...

Then...

Result

the system type is a three-pole circuit breaker with external neutral current transformer and without external neutral voltage tap

system type = 30

  • Measurements of the phase-to-phase voltages are available.

  • Measurements of the phase-to-neutral voltages are not available

  • Measurements of the neutral current is available.

  • 3 wattmeters method is not possible.

the system type is a three-pole circuit breaker without external neutral current transformer and without external neutral voltage tap

system type = 31

  • Measurements of the phase-to-phase voltages are available.

  • Measurements of the phase-to-neutral voltages are not available

  • Measurements of the neutral current is not available .

  • 3 wattmeters method is not possible.

the system type is a three-pole circuit breaker without external neutral current transformer and with external neutral voltage tap

system type = 40

  • Measurements of the phase-to-phase voltages are available.

  • Measurements of the phase-to-neutral voltages are available

  • Measurements of the neutral current is not available.

  • 3 wattmeters method is possible.

the system type is a three-pole circuit breaker with external neutral current transformer and external neutral voltage tap, or if the system type is four-pole circuit breaker

system type = 41

  • Measurements of the phase-to-phase voltages are available.

  • Measurements of the phase-to-neutral voltages are available

  • Measurements of the neutral current is available.

  • 3 wattmeters method is possible.

This table presents the text to choose on the ETV trip system display according to the system type determined previously:

If...

Then...

system type = 31

select 3W3ct

system type = 40

select 4W3ct

system type = 41

select 4W4ct

Power Flow Sign

Address

Register

RW

X

Unit

Type

Range

Description

0x0CF3

3316

R-W

INT16U

0–1

Power flow sign:

  • 0 = the active power flows from upstream (top) to downstream (bottom) (factory setting).

  • 1 = the active power flows from downstream (bottom) to upstream (top).

Demand Time

The current demand configuration command (command code = 47243) configures the content of registers 3351 and 3352.

The power demand configuration command (command code = 47244) configures the content of registers 3354 and 3355.

Address

Register

RW

X

Unit

Type

Range

Description

0x0D17

3352

R-WC

x1

min

INT16U

5–60

Duration of the current demand calculation window, adjustable in steps of 1 minute.
The factory setting is 15 minutes (1)

0x0D1A

3355

R-WC

x1

min

INT16U

5–60

Duration of the power demand calculation window, adjustable in steps of 1 minute.
The factory setting is 15 minutes.

(1) The duration in minutes of the current demand calculation window set in this register is used for the maximum current I1, I2, and I3, and IN protection functions. When these protection functions are active, it is possible to modify the duration of the calculation window whether the protective cover for the dial settings is closed or not, whether remote access is authorized (ETV trip system) or not, and whether the supervisor knows the remote access control word or not.

Nominal Voltage

The setup nominal primary voltage Vn display command (command code = 47245) configures the content of the nominal voltage register.

Address

Register

RW

X

Unit

Type

Range

Description

0x258F

9616

R-WC

1

V

INT16U

100–1150

Nominal primary voltage Vn on the voltage transformer.
Factory setting = 690 V

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.