DOCA0193EN-00

Protection Parameters

Neutral Protection Parameters

The neutral protection is only available when system type in register 3314 is 30 or 41 (refer to System Type).

Address

Register

RW

X

Unit

Type

Range

Description

0x2230

8753

R

1

INT16U

0–2

Type of neutral protection:
0 = OFF
1 = N/2 (Ir/2)
2 = N (Ir)

Long-Time Protection Parameters

Address

Register

RW

X

Unit

Type

Range

Bit

Description

0x2231

8754

R

INT16U

0–1

Status: 0x0001 = On

0x2232

8755

RW

INT16U

Type of IDMTL curve

0

Standard long-time curve I2t (factory setting)

1–15

Reserved

0x2233–0x2234

8756–8757

R

1

A

MOD10000

40–8000

Ir pick-up value

0x2235

8758

R

1

ms

INT16U

500–24000

tr time delay

0x2236–0x2239

8759–8762

Reserved

0x223A

8763

RW

INT16U

M2C programmable contact setting:
Bit set to 1 = contact closed at the end of the time delay tr (factory setting)
Bit set to 0 = contact open at the end of the time delay tr

0

Always set to 1

1–7

Reserved

8

Contact 1

9

Contact 2

10–15

Reserved

Short-Time Protection Parameters

Address

Register

RW

X

Unit

Type

Range

Bit

Description

0x223B

8764

R

INT16U

0–1

Status: 0x0001 = On

0x223C

8765

R

INT16U

0–1

Type of protection:
0 = I2t On
1 = I2t Off

0x223D–0x223E

8766–8767

R

A

MOD10000

60–80000

Isd pick-up value

0x223F

8768

R

ms

INT16U

0–400

tsd time delay
0 s: valid only for the I2t off position
100–400 ms: valid for the I2t on and I2t off positions

0x2240–0x2243

8769–8772

Reserved

0x2244

8773

RW

INT16U

M2C programmable contact setting:
Bit set to 1 = contact closed at the end of the time delay tsd (factory setting)
Bit set to 0 = contact open at the end of the time delay tsd

0

Always set to 1

1–7

Reserved

8

Contact 1

9

Contact 2

14–15

Reserved

Instantaneous Protection Parameters

Address

Register

RW

X

Unit

Type

Range

Bit

Description

0x2245

8774

R

INT16U

0x0001–0x0101

0x0001 = protection active (factory setting)
0x0101 = protection OFF

0x2246

8775

Reserved

0x2247–0x2248

8776–8777

R

1

A

MOD10000

200–120000

I pick-up value for the instantaneous protection

0x2249

8778

Reserved

0x224A–0x224D

8779–8782

Reserved

0x224E

8783

RW

INT16U

M2C programmable contact setting:
Bit set to 1 = contact closed at the end of the time delay (factory setting)
Bit set to 0 = contact open at the end of the time delay

0

Always set to 1

1–7

Reserved

8

Contact 1

9

Contact 2

14–15

Reserved

Ground-Fault Protection Parameters

Address

Register

RW

X

Unit

Type

Range

Bit

Description

0x224F

8784

RW

INT16U

0x0001–0x0101

Protection status:
0x0001 = protection active (factory setting)
0x0101 = protection OFF

0x2250

8785

R

INT16U

0–1

Type of protection:
0 = I2t On
1 = I2t Off

0x2251–0x2252

8786–8787

R

1

A

MOD10000

30–1200

Ig pickup for the ground-fault protection

0x2253

8788

R

1

ms

INT16U

0–400

tg tripping time delay for the ground-fault protection:
0 s = valid only for the I2t off position
100–400 ms = valid for the I2t on and I2t off positions

0x2254–0x2257

8789–8792

Reserved

0x2258

8793

RW

INT16U

M2C programmable contact setting:
Bit set to 1 = contact closed at the end of the time delay tg (factory setting)
Bit set to 0 = contact open at the end of the time delay tg

0

Always set to 1

1–7

Reserved

8

Contact 1

9

Contact 2

14–15

Reserved

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.