DOCA0193EN-00

IO Module Identification

Introduction

The order and the description of the IO module identification registers for IO 2 are the same as those of IO 1.

Addresses and Registers List

The following table describes the identification addresses, and registers regarding the IO module.

IO Module

Addresses

Registers

IO 1

0x392F–0x3982

14640–14723

IO 2

0x44E7–0x453A

17640–17723

IO Hardware Revision

The hardware revision is an ASCII string using the format XXX.YYY.ZZZ with:

  • XXX = major version (000–127)

  • YYY = minor version (000–255)

  • ZZZ = revision number (000–255)

The NULL character ends the revision number.

Address

Register

RW

Unit

Type

Range

Description

0x3961– 0x3966

14690–14695

R

OCTET STRING

Hardware revision

IO Module Firmware Revision

The hardware revision is an ASCII string using the format XXX.YYY.ZZZ with:

  • XXX = major version (000–127)

  • YYY = minor version (000–255)

  • ZZZ = revision number (000–255)

The NULL character ends the revision number.

Address

Register

RW

Unit

Type

Range

Description

0x3967–0x396C

14696–14701

R

OCTET STRING

Firmware revision

Current Date and Time

Address

Register

RW

Unit

Type

Range

Description

0x396D–0x3970

14702–14705

R

DATETIME

Current date and time of the IO module in DATETIME format.

The value is automatically updated when the DATETIME of IFM interface is set.

Serial Number

The IO module serial number is composed of a maximum of 11 alphanumeric characters with the following format: PPYYWWDnnnn.

  • PP = plant code

  • YY = year of fabrication (05–99)

  • WW = week of fabrication (01–53)

  • D = day of fabrication (1–7)

  • nnnn = production number of the device on the day (0001–9999)

A read request of six registers is necessary to read the IO module serial number.

Address

Register

RW

Unit

Type

Range

Description

0x3971–0x397A

14706-14715

R

OCTET STRING

Serial number

0x3971

14706

R

OCTET STRING

‘PP’

0x3972

14707

R

OCTET STRING

‘05’–‘99’

‘YY’

0x3973

14708

R

OCTET STRING

‘01’–‘53’

‘WW’

0x3974

14709

R

OCTET STRING

‘10’–‘79’

‘Dn’

0x3975

14710

R

OCTET STRING

‘00’–‘99’

‘nn’

0x3976

14711

R

OCTET STRING

‘0’–‘9’

‘n’ (the NULL character ends the serial number)

Manufacturing Date and Time

Address

Register

RW

Unit

Type

Range

Description

0x397B–0x397E

14716–14719

R

DATETIME

Manufacturing date and time

Product Identification

Address

Register

RW

Unit

Type

Range

Description

0x392F

14640

R

INT16U

15150

Product identification = 15150 for the IO module

0x3930

14641

Reserved

0x397F–0x3982

14720–14723

R

OCTET STRING

Product code = ‘LV434063’

0x3D1C–0x3D3B

15645–15676

R–WC

OCTET STRING

User application name

0x3D3C–0x3D45

15677–15686

R

OCTET STRING

Vendor name = ‘Schneider Electric’

0x3D46–0x3D4D

15687–15694

R

OCTET STRING

Product range: ‘Enerlinx’

0x3D4E–0x3D5D

15695–15710

R

OCTET STRING

Device family: ‘IO device’

0x3D5E–0x3D65

15711–15718

R

OCTET STRING

Product model

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.