DOCA0193EN-00

Time-Stamped Information

General Description

The time-stamped information enables to know all the dates relative to important information.

Date of Last Event

Address

Register

RW

X

Unit

Type

Range

Description

0x02A6–0x02A9

679–682

R

XDATE

Current date of BCM ULP module

0x02AB–0x02AD

684–686

R

DATE

Date of last circuit breaker opening

0x02AE–0x02B0

687–689

R

DATE

Date of last circuit breaker closing

0x02B1–0x02B3

690–692

R

DATE

Date of last trip without an electrical fault

0x02B4–0x02B6

693–695

R

DATE

Date of last trip with an electrical fault

0x02B7–0x02B9

696–698

R

DATE

Date of last “PF ready to close” status

0x02BA–0x02BC

699–701

R

DATE

Date of last “End of opening order” event. This event occurs when:

  • there is no action on the opening pushbutton on the front of the device

  • the fault-trip reset pushbutton is in (the device is reset)

  • the MN undervoltage release is powered (if present)

0x02BD–0x02BF

702–704

R

DATE

Date of last “CH spring charged” status

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.