DOCA0193EN-00

ETV Trip System Identification

Serial Number

Address

Register

RW

X

Unit

Type

Range

Description

0x21FB– 0x21FE

8700–8703

R

1

OCTET STRING

Serial number encoded in ASCII

Firmware Version

Address

Register

RW

X

Unit

Type

Range

Description

0x2205

8710

R

1

INT16

ETV trip system firmware version.
For example, the value 8244 corresponds to version 8.244.

Protection Type

Address

Register

RW

X

Unit

Type

Range

Description

0x2223

8740

R

1

OCTET STRING

20–70

Type of protection:
‘20’ = ETV 2I
‘50’ = ETV 5S
‘60’ = ETV 6G

Long-Time Rating Plug

Address

Register

RW

X

Unit

Type

Range

Description

0x2225

8742

R

1

INT16U

0–15

Type of long-time rating plug:
0 = missing
1 = IEC standard
2 = IEC low
3 = IEC High
7 = UL-A
8 = UL-B
9 = UL-C
10 = OFF
11 = UL-D
12 = UL-E
13 = UL-F
14 = UL-G
15 = UL-H

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.