DOCA0193EN-00

Status

M2C Programmable Contacts Status

The M2C status register indicates the status of the programmable contacts:

  • status bit = 0: the contact is open.

  • status bit = 1: the contact is closed.

The contact statuses are automatically updated, a reset is not possible.

Address

Register

RW

X

Unit

Type

Range

Bit

Description

0x229D

8857

R

INT16U

0

Contact 1 status

1

Contact 2 status

2–15

Reserved

Protection Status

The following table details the values for each bit of protection pick-up value registers:

  • protection status bit = 0: protection pick-up value is not overrun.

  • protection status bit = 1: protection pick-up value is overrun, even if the time delay has not expired.

Address

Register

RW

X

Unit

Type

Range

Bit

Description

0x229D

8862

R

INT16U

0

Long-time protection status

1–15

Reserved

0x229E

8863

Reserved

0x229F

8864

R

INT16U

0

Ground-fault alarm status

1–15

Reserved

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.