DOCA0193EN-00

Configuration

General Description

The IFM interface integrates automatic configuration (Auto-Speed sensing ON, factory setting). When connected to the Modbus network, the IFM interface automatically detects the network parameters.

Automatic Configuration

The Modbus slave address is defined by the two address rotary switches on the front panel of the IFM interface. When connected to the Modbus serial line network, the IFM interface automatically detects the network speed and parity. The Auto-Speed sensing algorithm tests the available Baud rates and parities, and automatically detects the Modbus communication network parameters. The Modbus master must send at least 25 frames on the Modbus network to allow the Auto-Speed sensing algorithm to work.

The transmission format is binary with one start bit, eight data bits, one stop bit in case of even or odd parity, and two stop bits in case of no parity.

If the Auto-Speed sensing algorithm does not detect the network parameters, it is recommended to follow this procedure:

1

Set up the IFM interface to Modbus address 1 (refer to Modbus Address Rotary Switches).

2

Send a read multiple register request (function code 0x03) to slave 1, at any address and for any number of registers.

3

Send this request at least 25 times.

NOTE: If the network speed or parity is changed after the IFM interface has automatically detected these settings, the IFM interface must be restarted (power off and on) to detect the new network parameters.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.