DOCA0193EN-00

Counters

General Description

The BCM ULP module has counters that help managing the circuit breaker.

The BCM ULP module counters have the following properties:

  • All the counters are saved in non-volatile memory to prevent data loss in case of power loss.

  • The cumulating OF counter is read only. It stops incrementing when it reaches the maximum value of 65535.

  • All counters (except the cumulating OF counter) can be preset to any value from 0 to 65535. The counters automatically cycle from 65535 to 0.

  • A threshold is associated to the OF counter and to the close circuit breaker command counter. The thresholds can be set to any value from 0 to 65534. The factory setting is 5000. An alarm is generated when a counter reaches the threshold.

BCM ULP Module Counters

Address

Register

RW

X

Unit

Type

Range

Description

0x0229

554

R

INT16U

0–65535

Counter for the number of times the BCM ULP module is energized

0x022A

555

R

INT16U

0–65535

Counter for the number of times the BCM ULP module is reset whether following power loss or not

Counter Thresholds

Address

Register

RW

X

Unit

Type

Range

Description

0x0243

580

RW

INT16U

0–65535

OF counter threshold
Factory setting = 5000

Circuit Breaker Operation Counters

Address

Register

RW

X

Unit

Type

Range

Description

0x0295

662

R

INT16

0–65535

Cumulating OF counter (non-resettable open to close counter)

0x0296

663

RW

INT16

0–65535

OF counter (resettable open to close counter)

0x0297

664

RW

INT16

0–65535

SD counter (close to SD position)

0x0298

665

RW

INT16

0–65535

SDE counter (close to SDE position)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.