DOCA0193EN-00

List of ETV Trip System Commands and Error Codes

List of Commands

The following table lists the available ETV trip system commands, their corresponding command codes, and user profiles. Follow the command execution procedures accordingly (refer to Executing a Command):

Command

Command Code

User Profile

Set up ENVT presence (refer to Set Up ENVT Presence)

46472

Administrator

Reset minimum/maximum (refer to Reset Minimum/Maximum)

46728

Administrator or Operator

Current demand configuration (refer to Current Demand Configuration)

47243

Administrator

Power demand configuration (refer to Power Demand Configuration)

47244

Administrator

Set up nominal voltage Vn display (refer to Set Up Nominal Primary Voltage Vn Display)

47245

Administrator

Error Codes

Error codes generated by ETV trip systems are the generic error codes (refer to Result of the Command).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.