DOCA0193EN-00

Energy Measurements

General Description

Energy measurements include:

  • active energy Ep

  • reactive energy Eq

  • apparent energy Es

Address

Register

RW

X

Unit

Type

Range

Description

0x07CF–0x07D2

2000–2003

RW

1

kWh

MOD10000

-1016 to +1016

Total active energy: Ep(1)

0x07D3–0x07D6

2004–2007

RW

1

kVARh

MOD10000

-1016 to +1016

Total reactive energy: Eq(1)

0x07D7–0x07E6

2008–2023

Reserved

0x07E7–0x07EA

2024–2027

RW

1

kVAh

MOD10000

-1016 to +1016

Total apparent energy: Es

(1) Total active energy and total reactive energy are always counted positively with ETV trip system.

NOTE:
  • The ETV trip system screen displays positive values (only) up to 999 999 999 kWh. Over this value, the ETV trip system screen displays 999 999 999 kWh.

  • MOD10000 format is explained in the data type description (refer to Data Type: MOD10000).

The behavior is the same for reactive energy and apparent energy.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.