DOCA0193EN-00

Digital Outputs

Digital Output Register Mapping

Each digital output description is made up of 60 registers. The order and the description of the digital outputs 2 and 3 are the same as those of digital output 1.

IO Module

Digital Output Number

Digital Output Addresses

Digital Output Registers

IO 1

O1

0x3849–0x3884

14410–14469

O2

0x3885–0x38C0

14470–14529

O3

0x38C1–0x38FC

14530–14589

IO 2

O1

0x4401–0x443C

17410–17469

O2

0x443D–0x4478

17470–17529

O3

0x4479–0x44B4

17530–17589

Digital Output 1 Registers of IO 1

The order and the description of the digital output 1 registers of IO 2 are the same as those of IO 1:

Address

Register

RW

Unit

Type

Range

Bit

Description

0x3849

14410

R

INT16U

Quality of each bit of register 14411:

  • 0 = Invalid

  • 1 = Valid

0x384A

14411

R-WC

INT16U

0

Reserved

1

Digital output status:

  • 0 = OFF

  • 1 = ON

R

2

Digital output forced status:

  • 0 = Unforced

  • 1 = Forced

3–15

Reserved

0x384B–0x384E

14412–14415

R

DATETIME

Time-stamp for the last output transition:

  • Last rising edge if output is configured as NO (normally open contact)

  • Last falling edge if output is configured as NC (normally closed contact)

0x384F–0x3850

14416–14417

Reserved

0x3851–0x3852

14418–14419

R

INT32U

1-4294967294

Output counter
This counter increments for each rising edge of the output.

0x3853–0x3856

14420–14423

R

DATETIME

Time-stamp of the last reset for the output counter

0x3857–0x386E

14424–14447

R

OCTET STRING

Digital output identification coded over 45 ASCII characters

0x386F

14448

R

INT16U

0–2

Output operating mode(1):

  • 0 = Non-latching (factory setting)

  • 1 = Latched

  • 2 = Time delayed non-latching

0x3870

14449

R

s

INT16U

0–65534

On time for time delayed non-latching mode value(1).
The time for the output to remain energized when the output is in time delayed non-latching mode (Factory setting = 0)

0x3871

14450

R

INT16U

0–1

Output contact type:

  • 0 = NO (normally open, factory setting)

  • 1 = NC (normally close)

0x3872

14451

R

INT16U

0–2

Indicates On/Off state of the discrete output when any fall back condition occurs:

  • 0 = OFF (factory setting)

  • 1 = ON

  • 2 = Freeze

0x3873–0x3874

14452–14453

R

INT32U

1-4294967294

Output counter threshold value(1)
Factory setting = 5000

0x3875

14454

R

INT16U

0–2

Simple command for output(1):

  • 0 = No command

  • 1 = OFF

  • 2 = ON

Valid if simple commands are enabled.

0x3876–0x3884

14455–14469

Reserved

(1) Contact Schneider Electric field service representative to set the value.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.