DOCA0193EN-00

Password Management

Remote access to data on ETV trip systems and the ULP modules by using the communication network is protected by password.

Four user profiles are defined for remote access. Each IMU has a different password for each user profile. The password for each user profile is as follows:

User Profile

Password

Administrator

‘0000’=0x30303030

Services

‘1111’=0x31313131

Engineer

‘2222’=0x32323232

Operator

‘3333’=0x33333333

Each intrusive command via the command interface is assigned to one or several user profiles, and protected by the corresponding user profile password. The password for each intrusive command is indicated in the description of the command.

No password is required for non-intrusive commands through the command interface.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.