DOCA0193EN-00

Configuration of the M2C Programmable Contacts

General Description

The M2C has two programmable contacts, 1 and 2, that may be used to signal pick-up value overruns or status changes.

The M2C programmable contacts can be configured remotely via the communication interface.

M2C Programmable Contact Registers

The settings of the M2C programmable contacts are in the contact registers:

Contact Number

Contact Addresses

Contact Registers

1

0x2648–0x264E

9801–9807

2

0x264F–0x2655

9808–9814

M2C Programmable Contact 1 Description

The order and the description of the M2C programmable contact 2 is the same as that of contact 1:

Address

Register

RW

X

Unit

Type

Range

Description

0x2648

9801

RW

INT16U

0–4

Output mode

0 = normal (non-latching) mode (factory setting)

Contact closed each time for as long as the assigned alarm remains active.

3 = forced to 1

The contact remains closed and is not controlled by the alarm status.

4 = forced to 0

The contact remains open and is not controlled by the alarm status

0x2649–0x264D

9802–9806

Reserved

0x264E

9807

RW

INT16U

1000–1031

Owner alarm number for the contact 1.

Factory setting = 0x8000 (no owner)

Type of Programmable Contacts

Address

Register

RW

X

Unit

Type

Range

Description

0x2672

9843

R

INT16U

0–6

0 = none

2 = M2C

Event Assignment to M2C Programmable Contacts

The M2C programmable contacts can be associated to a protection parameter event.

Depending on the protection parameter, a specific register can contain the programmable contact number which opens or closes at the end of the protection time delay (register 8763 as example).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.