DOCA0343EN-02

Cord and Plug Connections

NOTICE
Wire insulation damage
  • Ensure that all pathways and raceways used for routing and storing conductors are free of rough, sharp, or moving parts to prevent damage to conductor insulation.
  • Ensure that the connectors are inserted properly to avoid any loose connections.
  • Ensure that the striped wire length is as per the specifications given in the manual. The screws are fastened to ensure the reliability of connections.
Failure to follow these instructions can result in equipment damage.
NOTE:
  • Use a Class 2 external power supply in case the supplied power supply is not being used.

  • Follow the install instructions of the power supply used.

  • For the DC connections of the Flex-Server. refer to the instruction sheet.

  • Use a heat shrink tube to secure the loose insulated conductors.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?