Network Priority Configuration (Flex-Server)
The Flex-Server follows a predefined interface priority for internet connectivity. This priority determines which network interface the server uses when multiple options are available. Currently, USB takes the highest precedence, followed by the order: GSM > Ethernet > Wi-Fi.
Priority Order
The current interface priority order is:
-
USB (highest priority)
-
GSM
-
Ethernet
-
Wi-Fi
Common Field Use Cases
|
Use Case |
GSM |
Ethernet |
Wi-Fi |
|---|---|---|---|
|
1 |
✔ |
✔ |
– |
|
2 |
– |
✔ |
– |
|
3 |
✔ |
– |
✔ |
|
4 |
– |
✔ |
✔ |
Configuration Notes
Review the following configuration details.
-
GSM
The server automatically handles GSM configuration; no dashboard configuration is necessary.
For more information, refer to Support New SIM Cards in the Field section.
-
Ethernet and Wi-Fi
If you are using only Ethernet or Wi-Fi to bring the server online, DHCP configuration is sufficient.
If you are using these interfaces to communicate with devices, we recommend static IP configuration.
Static IP configuration is a prerequisite for proper equipment and device communication setup.
Future Scope
The ability to view and change interface priority directly from the dashboard will be introduced in future releases.