DOCA0343EN-02

Introduction

The Local Web Dashboard (LWD) is a web-based interface that allows users to access and configure the Flex-Server over an Ethernet connection. It is compatible with major web browsers like Chrome, Firefox, Safari, and Edge.

Through the web dashboard, users can:

  • Manage network settings

  • View hardware information

  • Override equipment settings (post-commissioning)

NOTE:
  1. By default, LWD is not enabled on any Flex-Server.

  2. To configure or use LWD, the user must request the support team to enable it for their Flex-Server.

  3. Once enabled, it is strongly recommended that the user logs in to LWD and changes the default password immediately.

  4. If a site has multiple Flex-Server’s (like 3 or 4 servers), the user must request LWD to be enabled on each server individually.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?