DOCA0343EN-02

Peripheral Mapping

The Peripheral Mapping section consists of four configuration cards:

  • Internal Connector - Displays devices connected to the Flex-Server.

    • M.2 Slot - If set to Wi-Fi Adapter, the Flex-Server supports Wi-Fi connectivity. If set to None, Wi-Fi is not available.

    • mPCIe Slot - If configured with a 4G modem, the Flex-Server can connect to a SIM network; otherwise, it cannot.

    • SIM Slot - Selecting the incorrect SIM slot may prevent the Flex-Server from coming online.

  • On-Board (RS485) - Serial Port Configuration.

    The RS485 port supports either Modbus RTU or BACnet MSTP connections.

    • If using Modbus RTU:

      • Priority (Set priority for communication)

      • Baud Rate (Speed of data transmission)

      • Stop Bit (Defines stop bit configuration)

    • If using BACnet MSTP:

      • Gateway Address

      • Baud Rate

  • USB Ports Configuration (Top and Bottom).

    • USB (Top): Functions similarly to the On-Board RS485 port.

    • USB (Bottom): Functions similarly to the On-Board RS485 port.

  • Using LoRaWAN (Top and Bottom).

    • Select Protocol as LoRaWAN.

    • Select Region from the dropdown as per the country.

Future Scope

  • Allows you to enter PIN, username, and password for SIM authentication.

  • Enable you to set default network priority from the dashboard.

  • Expand USB port support for additional protocols.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?