DOCA0343EN-02

How to Use the Device Hub

Accessing the Device Hub

  1. Go to the main menu on the left side of the Deployment Portal.

  2. Click Device Hub to open the device listing page.

Viewing the Device List

  1. The landing page displays a paginated list of devices with the following columns:

    • Model
    • Manufacturer
    • Description
    • Protocol
    • Verified

  2. Use the pagination controls at the bottom to navigate through multiple pages.

Searching for a Device

  1. Use Search option at the top of the list.

  2. Enter keywords such as Model name or Protocol to narrow the results.

Filtering Devices

  1. Click icon next to any column header (for example, Protocol or Manufacturer).

  2. Select your desired criteria to filter the list.

Viewing Detailed Device Parameters

  1. Click any row in the device list to open the detailed view.

  2. The detail page includes the device’s parameter list and its mapping template.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?