DOCA0343EN-02

Device Plots

The Plotter feature helps visualize various data streams available on devices, equipment, and the Flex-Server. Follow the steps below to view and analyse data.

NOTE: Only Active devices will be visible here.

You can select Customer and Site.

After selecting the customer and site, two options will be displayed.

  1. Device Tab (selected by default)

  2. Equipment Tab

    NOTE: By default, selected as Device tab.

Switch between the two tabs based on the data which you need to view.

Follow the steps below to set the default plot for both the Device and Equipment tabs:

  1. Date Range: Today, from 12:00 AM to current server local time

  2. Aggregation: Operator Mean

  3. Time Interval: 1 minute

Using Device Tab

  1. Click server’s name to view all associated to devices.

  2. Click device name to see its parameters.

  3. Select the point(s) to view.

  4. Click Apply.

Using Equipment Tab

  1. Click equipment name to view parameters listed by display name.

  2. Select the point(s) to view.

  3. Click Apply.

NOTE: For both tabs, use the option to set and view parameters such as Gateways, Protocols, Equipment Type, and more.

Search Functionality

Global search: Global Search refers to a unified search functionality that allows you to search across multiple data sources, modules, or sections within a system or application from a single search bar or interface. It provides a centralized way to retrieve relevant information - such as documents, records, users, settings, or content - regardless of where it is stored within the platform.

Use the Global Search to search by:

  1. Device Name

  2. Parameter Name

  3. Equipment Name
  4. Equipment Type

Post-Plot Features

Once the data is plotted, user can view the following list of parameters:

  1. Click icon to view meta information.

  2. Click icon to hide/unhide parameters.

  3. Click icon to remove a parameters.

  4. Plot a maximum of 10 parameters at once.

  5. Select up to 3 axes for plotting based on the data type.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?