DOCA0343EN-02

Device Hub

Overview

The Device Hub page provides a comprehensive list of templatized devices available in the Deployment Portal. It includes detailed information about each device, such as Model, Manufacturer, Description, Protocol, and Verified verification status. You can filter and search devices, and view mapping details for each device and download the list of devices.

Key Features

  • Comprehensive device listing: Displays all registered devices with key details such as Model, Manufacturer, Description, Protocol, and Verified verification status.

  • Search and filter capabilities: Easily search and apply filters to quickly locate specific devices.

  • Device Verification Status Indicators:

    • indicates the device data has been evaluated and successfully integrated.

    • indicates the device is integrated, but its data has not been evaluated yet.

  • Parameter-Level Details: Click a device entry to reveal parameters details and mapping templates.

  • Download: Click icon located at the top right corner to download the list of all devices.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?