Regulatory Compliance
FCC Compliance Statement (USA)
ESXBFXSVRBCW008: ESXB Flex-Server, Ethernet, RS485, cellular, Wi-Fi, 8GB storage
FCC ID: 2BATG- ESXBFXSVRBCW
ESXBFXSVR0BC008: ESXB Flex-Server, Ethernet, RS485, cellular, 8GB storage
FCC ID: 2BATG- ESXBFXSVR0BC
Compliance Statements: This device complies with Part 15 of the FCC Rules. Operation is subject to the following two conditions:
-
This device may not cause harmful interference.
-
This device must accept any interference received, including, an interference that may cause undesired operation.
Caution Statements:
-
Any changes or modifications not expressly approved by the party responsible for compliance could void the user’s authority to operate this equipment.
-
This equipment should be installed and operated with a minimum distance of 200 mm between the radiator and your body.
Industry Canada (IC) Compliance Statement
ESXBFXSVRBCW008: ESXB Flex-Server, Ethernet, RS485, cellular, Wi-Fi, 8GB storage
IC: 30486-FXSVRBCW
ESXBFXSVR0BC008: ESXB Flex-Server, Ethernet, RS485, cellular, 8GB storage
IC: 30486-FXSVR0BC
Compliance Statements: This device complies with Industry Canada license exempt RSS standard(s). Operation is subject to the following two conditions:
-
This device may not cause interference.
- This device must accept any interference, including interference that may cause undesired operation of the device.
Déclarations de conformité: Le présent appareil est conforme aux CNR d’Industrie Canada applicables aux appareils radio exempts de licence. L’exploitation est autorisée aux deux conditions suivantes:
-
l’appareil ne doit pas produire de brouillage, et.
-
l’utilisateur de l’appareil doit accepter tout brouillage radioélectrique subi, même si le brouillage est susceptible d’en compromettre le fonctionnement
Caution Statements:
-
This equipment complies with radio frequency exposure limits set forth by Industry Canada for an uncontrolled environment.
-
This equipment should be installed and operated with a minimum distance of 200 mm between the device and the user or bystanders.
Déclarations de mise en garde:
-
Cet équipement est conforme aux limites d'exposition aux radiofréquences défines par Indstrie Canada pourun environment non contrôlé.
-
Cet équipement doit être installé et utilisé aven un minimum de 20 cm de distance dispositif et l'utilisateur ou des tiers.
INFORMATION TO THE USER
For Class A and Class B digital devices, information to the user is required to include the following statements (Section 15.105):
-
For a Class A digital device or peripheral, the instructions furnished to the user shall include the following or similar statement, placed in a prominent location in the text of the manual:
NOTE: This equipment has been tested and found to comply with the limits for a Class A digital device, pursuant to part 15 of the FCC Rules. These limits are designed to provide reasonable protection against harmful interference when the equipment is operated in a commercial environment. This equipment generates, uses, and can radiate radio frequency energy and, if not installed and used in accordance with the instruction manual, may cause harmful interference to radio communications. Operation of this equipment in a residential area is likely to cause harmful interference in which case the user will be required to correct the interference at his own expense. -
For a Class B digital device or peripheral, the instructions furnished to the user shall include the following or similar statement, placed in a prominent location in the text of the manual:
NOTE: This equipment has been tested and found to comply with the limits for a Class B digital device, pursuant to part 15 of the FCC Rules. These limits are designed to provide reasonable protection against harmful interference in a residential installation. This equipment generates, uses and can radiate radio frequency energy and, if not installed and used in accordance with the instructions, may cause harmful interference to radio communications. However, there is no guarantee that interference will not occur in a particular installation. If this equipment does cause harmful interference to radio or television reception, which can be determined by turning the equipment off and on, the user is encouraged to try to correct the interference by one or more of the following measures:
-
Reorient or relocate the receiving antenna.
-
Increase the separation between the equipment and receiver.
-
Connect the equipment into an outlet on a circuit different from that to which the receiver is connected.
-
Consult the dealer or an experienced radio/TV technician for help.