DOCA0343EN-02

New Device

The New Device screen is used for configuring new devices.

Add New Device

To add a device, follow the steps below:

  1. Select a protocol from the menu.

  2. After you select a protocol, proceed to add devices.

You can add multiple devices of the same protocol at once. The system displays all newly added devices in a list below, allowing you to review and submit them together.

NOTE: To remove a device before creating it, click Delete to remove it from the list before submission.

This process reduces the need to repeatedly enter the same information and minimizes configuration effort.

Future Scope

  • Expand device list with additional details.

  • Allows you to add more ports for BACnet IP and Modbus TCP/IP.

  • Enable device unit configuration in the template or scan flow.

  • Provide functionality to edit templates by removing or adding parameters.

  • Introduce an Upload Points feature.

  • Enable BACnet MSTP scanning.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?