DOCA0343EN-02

Existing Server

Enable server: Server and associated devices will be visible on deployment portal and other like Customer Portal.

Disable server: Server will shift into the disabled list and user cannot access the associated devices and equipment in troubleshooting section on deployment portal and it will be also removed from Customer Portal.

  1. To disable/enable the server, click toggle right side on top of the server card.
  2. To delete the server from the site, click and type DELETE in uppercase letters.
    NOTE: Enabling or disabling the server will automatically submit to the backend within 5 minutes. No manual submission is required.
  3. Click Delete.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?