DOCA0343EN-02

System Requirements

The System requirements section provides the necessary information about the Hardware, Software and Network .

Hardware

  • A laptop with an Ethernet port or Ethernet-to-USB adapter

  • A standard Ethernet cable

  • A server with a pre-defined static IP address.
    (IP can found in the Network Configuration section of the dashboard)

    NOTE: If the server does not configure with static IP address, then you can assign one through the dashboard interface after initial access.

Software

  • A modern web browser (Chrome, Firefox, Safari, or Edge).

Network

  • Access to server’s IP address (available on deployment portal).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?