Dashboard Navigation
Overview
The Home Page of the Local Web Dashboard (LWD) provides a quick navigation panel to access key configuration and control options for your Flex Server. From Home Page, users can Access Network Configuration, Server Management, User Configuration, and Equipment Controls.
The home screen offers panels for:
-
Network Settings: Ethernet, Wi-Fi, and SIM configuration
-
Hardware Info: MAC Address, Serial Number, and SPIN Version
-
Control Screen: Manage and sync equipment with cloud data
Network Configuration
Ethernet Configuration: Manage static IP, DNS, router IP, and protocol type.
Static IP flow
|
Field |
Description |
Example |
|
IP |
Static IP address |
192.168.0.150 |
|
DNS |
DNS server address |
8.8.8.8 |
|
Router IP |
Default gateway/router address |
192.168.0.1 |
|
Protocol |
Set to Static for manual network settings |
Static |
DHCP flow
|
Field |
Description |
Example |
|
Protocol |
Set to DHCP for automatic IP configuration |
DHCP |
Wi-Fi Configuration: Configure SSID, password, router IP, DNS, and protocol (DHCP/static).
Static IP flow
|
Field |
Description |
Example |
|
SSID |
Wireless network name |
Office_WiFi_01 |
|
Password |
Wi-Fi Password |
securewifi2024 |
|
Router IP |
Default gateway for Wi-Fi network |
192.168.43.1 |
|
DNS |
DNS server address |
8.8.4.4 |
|
Protocol |
Set to Static for manual network settings |
Static |
|
Password Status |
Toggle to enable/disable password authentication |
True |
DHCP flow
|
Field |
Description |
Example |
|
SSID |
Wireless network name |
Guest_Network |
|
Password |
Wi-Fi password (if Password Status is True) |
welcome123 |
|
Protocol |
Set to DHCP for automatic IP settings |
DHCP |
GSM Top / GSM Bottom Configuration: Set APN, Username, Password, PIN, and View activation status for cellular connectivity.
|
Field |
Description |
|
APN |
Access Point Name for network connectivity |
|
Username |
SIM username (if provided by network) |
|
Password |
SIM password (if provided by network) |
|
PIN |
SIM PIN (if applicable) |
Server Management/Hardware Details
The Hardware Details section provides essential information about the device's network interface, onboard compute module, and installed SIM card.
|
Field |
Description |
|---|---|
|
MAC Address |
Displays unique hardware address of the device’s network interface. |
|
Serial Number |
Displays unique identifier assigned to the hardware by the manufacturer. |
|
SPIN Version |
Displays version number of the SPIN software currently running on the device. |
|
Compute Module Number |
Displays identifier for the onboard compute module inside the device. |
|
SIM Number |
Displays unique number associated with the SIM card installed in the device. |
Control Screen
The Controls section of the Local Web Dashboard (LWD) allows users to view and manage operational controls for equipment connected to the current Flex-Server.
|
Field |
Description |
|---|---|
|
Unit Preference |
Select the preferred measurement system (Imperial/Metric). |
|
Select Equipment Type |
Choose the equipment type available under the current Flex-Server. |
|
Equipment Name |
Displays the name of the connected equipment. |
|
ON/OFF Control |
Shows the current operational status (ON/OFF Control) of the equipment. |
|
Control Type |
Displays the control method – typically Override. |
Click the Edit icon() next to the Control Type to apply a temporary
Override.
You can select one of the following durations for the override:
-
30 Minutes
-
1 Hour
-
2 Hours
The selected ON/OFF Control state will remain active for the chosen period, after which it will automatically return to its scheduled or default behaviour.
-
User can view list of equipment synced from the cloud.
-
User can verify equipment name, override duration and status.
-
Equipment names are read-only on the local dashboard and can only be edited from the cloud.
-
All control actions on the Local Web Dashboard (LWD) are automated.
-
Any configuration changes on the LWD require a rollout from the cloud, as the dashboard operates on the edge.
-
Only parameters with Actuation Type: True and Visibility: True will be displayed for the selected equipment on the LWD.
-
Only equipment under the current Flex-Server will be visible – no cross- Flex-Server equipment will appear on this dashboard.