DOCA0343EN-02

Add a LoRaWAN Device

  1. On the Devices page, click New Device > On Site.
  2. Select Protocol as LoRaWAN.
  3. Select the desired Server.
  4. Enter a unique Device Name to be displayed on the dashboard.
  5. Enter DevEUI and JoinEUI/AppEUI. Both DevEUI and JoinEUI/AppEUI should be case-sensitive, hexadecimal, must be exactly 16 characters.
  6. Enter App Key. The App Key should be case-sensitive, hexadecimal, must be exactly 32 characters.
  7. Enter the Data Rate (in minutes).
  8. The region configured in the peripheral mapping will be displayed here. To modify the region information, click the Settings icon located at the top-right corner of the screen and update the peripheral mapping.
  9. Click Add.
  10. To add another Device, enter a unique Address, Device Name, DevEUI, App Key and then click Add.
  11. Once you have added all devices, click Next.
  12. In the Template, search for the device model.
  13. Select the relevant Template. Verify the chosen Template shown below to ensure it is correct.
  14. Check if the Device uses SI Units or Imperial Units. The dashboard stores the data in SI Units by default. Convert values if needed:
    1. Select the parameters in the table.
    2. Click Convert to Metric to switch to SI Units.
    3. If necessary, click Undo to revert the changes.
  15. Click Mark as Completed to save the configuration.
  16. Click Next to go to the Existing Devices list.
  17. Select the check box next to the server’s name to include all modified or newly added devices.
  18. Clear the box which is not necessary to send to the Flex-Server.
  19. Click Next at the bottom right to submit the configuration.
    For more details on submitting configurations, refer to the Existing Device, page 44 section.
    NOTE: Read and Write action functionality is not applicable for LoRaWAN protocol.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?