DOCA0343EN-02

Provisioning the Flex-Server

Perform the following steps to provision the Flex-Server.
  1. Power on the Flex-Server by connecting it to the power source using the power cable provided inside the box.
  2. Wait for the top LED on the Flex-Server to start blinking green, this process may take up to 5 minutes.
    NOTE: The inserted SIM automatically connects the Flex-Server online and if the Flex-Server does not come online then manual intervention is needed. The option to choose between Wi-Fi or Ethernet is available in the later stages.
  3. Visit the partner portal dashboard.
  4. Sign in to the Deployment Portal.
  5. Click Deployment tab.
  6. Select customer from Select a customer menu.
    The list of associated sites appears.
    • If no server is associated with a site, the system displays: No server provisioned yet

    • A list of Flex-Server’s associated with the site appears.

  7. Configure a Flex-Server. For more information, refer to Configure Flex Server.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?