Existing Equipment

The Existing Equipment section displays all configured equipment. The Equipment table has these columns:
-
Equipment Point Name: A display name that customers easily understand.
-
Device Point: The device object/parameter as the device provides it and as configured in the system.
-
Controllable: Indicates whether the equipment point is controllable (Yes/No).
-
Customer Controllable: Specifies if the customer can control the equipment (Yes/No).
-
Action: Provides an option to delete an Equipment Point Name.

Viewing and Editing Equipment
You can view a list of all equipment by display name.
-
Click equipment item to opens a detailed view of its configured device points.
-
Click Edit to add more points.
-
If an incorrect Equipment Type or Equipment Template was selected, you can delete and reconfigure the equipment.
Adding Device Points to Equipment

-
Click Add Point to search for an Equipment Point Name.
-
Use the search box to search all the available Equipment Point Name in the system.
NOTE: If an Equipment Point Name is missing, raise a request with the administrator. -
To select a Device Point, follow the below steps:
-
Search for the required point and view its full path, including device and server details.
-
Select the Server, then the Device, and finally choose the desired point, if you are not sure about the exact point name.
-
-
Click Save to confirm the configuration.