DOCA0343EN-02

Troubleshooting Tips

If the dashboard's connectivity fails, follow the below steps and re-connect.

  • Check Cable Connection: Make sure the cables are connected properly on both ends.

  • Disable Wi-Fi: Turn off active wireless networks to avoid IP conflicts.

  • Verify IP Configuration: Check that your laptop IP address is entered correctly.

  • Review Firewall Settings: Allow access to your security software or firewall.

  • Restart Devices: Restart both laptop and server.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?