DOCA0343EN-02

Add a New Flex-Server

  1. Click New Server and fill in the following details:
    1. Server Type: Select Flex-Server (currently the only option available).
    2. Server Name: Enter a display name for the Flex-Server.
    3. Carrier Board Serial Number: Enter the serial number from the sticker on the Flex-Server.
    4. Compute Module Serial Number: Enter the compute module serial number from the sticker.
    5. Fitting Location: Indicate the physical location where the Flex-Server is installed.
    6. Data Rate: Select 60 from the drop - down menu.
      Note: Currently set to a default publishing rate of 60 seconds (not configurable).
  2. Proceed to Network and Peripheral Configuration.
    After entering the required details, you will be automatically redirected to the Network and Peripheral Configuration section to continue the setup.
    1. If the server is unreachable, you will not be redirected to the Network and Peripheral Configuration page.
    2. In this case, if you navigate away from the screen, you will find the server card in the existing tab with a button labelled Check Status.
    3. Clicking Check Status will attempt to restart the provisioning process.
    4. If the server is online, you will be redirected to the Network Configuration screen to proceed with the setup
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?