DOCA0343EN-02

Configure Flex-Server

To configure a Flex-Server, follow the below steps:
  1. Click view on the right of the selected site.
    The system displays two sections:
    • Site Information: This section shows the Site name, Site Location, Latitude, and Longitude.

      NOTE: These parameters are pre-configured through backend and not by the user.
    • Server Information: This section contains two options:

      • Existing Server: Displays all configured servers if a server is already configured.

      • New Server: User must fill all the data. For more information, refer to Add a New Server.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?