DOCA0343EN-02

Devices

This interface allows you to manage devices, showing existing devices and providing options to add new ones

Interface Overview

The Devices interface is divided into two main sections:

  • Existing Device: Displays all configured devices, grouped by the server. For more information, refer to Existing Device.
  • New Device: Allows you to add new devices using the following supported protocols:
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?