DOCA0302EN-04

Details of Modbus Functions

Overview

This appendix describes Modbus functions supported by the I/O Smart Link device that are not available on the www.modbus.org website. It is not attempting to describe the whole protocol.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?