DOCA0302EN-04

Acti 9 Devices with Ti24 Interface

Overview

Devices (iACT24, iATL24, iOF+SD24, OF+SD24, RCA iC60, Reflex iC60) can be connected to the I/O Smart Link with EcoStruxure communication system pre-asssembled cables.

Wiring

The following figure shows the connection of devices to the I/O Smart Link using pre-assembled cables:

NOTE: A9XCAU06 or A9XCAC01 cable could be used to link Acti 9 devices with Ti24 interface to I/O Smart Link.

In this case, for the connection of iACT24 and iATL24, input I2 must be connected to both ends of A9XCAU06 or A9XCAC01 cable.

For detailed information regarding installation instructions, refer to PKR5509302 I/O Smart Link - Instruction Sheet.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?