Global Modbus Address Table
Presentation
|
Address Groups |
Description |
Address |
Register |
No. of Words |
Type |
RW |
|---|---|---|---|---|---|---|
|
System |
Serial number |
0x0064 |
101 |
6 |
ASCII |
R |
|
Status |
0x0070 |
113 |
2 |
BITMAP |
R |
|
|
Date and Time |
0x0073 |
116 |
4 |
DATE |
RW |
|
|
Hardware and firmware versions |
0x0086 |
135 |
18 |
ASCII |
R |
|
|
Identification |
0x01F4 |
501 |
109 |
ASCII |
R |
|
|
Summary of channels 1 to 11 |
Status |
0x0078 |
121 |
2 |
BITMAP |
R |
|
Orders |
0x0082 |
131 |
4 |
BITMAP |
RW |
|
|
Power or flow indicators |
0x36B0 |
14001 |
44 |
Float32 |
R |
|
|
Consumption meters |
0x36E2 |
14051 |
44 |
UINT32 |
R |
|
|
Operation counters |
0x3714 |
14101 |
44 |
UINT32 |
RW |
|
|
Running hour counters |
0x3740 |
14145 |
22 |
UINT32 |
RW |
|
|
Detail of channel 1 |
Status |
0x3778 |
14201 |
1 |
BITMAP |
R |
|
Orders |
0x3779 |
14202 |
2 |
BITMAP |
RW |
|
|
Output status |
0x377B |
14204 |
1 |
BITMAP |
R |
|
|
Power or flow indicators |
0x377C |
14205 |
4 |
Float32 |
R |
|
|
Consumption meters |
0x3780 |
14209 |
4 |
UINT32 |
R |
|
|
Operation counters |
0x3784 |
14213 |
4 |
UINT32 |
RW |
|
|
Running hour counters |
0x3788 |
14217 |
2 |
UINT32 |
RW |
|
|
Setting date of operation counters |
0x378A |
14219 |
12 |
DATE |
R |
|
|
Pulse weight settings (meters) |
0x3796 |
14231 |
2 |
UNIT |
RW |
|
|
Detail of channels 2 to 11 |
Channel 2(1) |
0x37a0 |
14241 |
40 |
– |
– |
|
Channel 3(1) |
0x37c8 |
14281 |
40 |
– |
– |
|
|
Channel 4(1) |
0x37f0 |
14321 |
40 |
– |
– |
|
|
Channel 5(1) |
0x3818 |
14361 |
40 |
– |
– |
|
|
Channel 6(1) |
0x3840 |
14401 |
40 |
– |
– |
|
|
Channel 7(1) |
0x3868 |
14441 |
40 |
– |
– |
|
|
Channel 8(1) |
0x3890 |
14481 |
40 |
– |
– |
|
|
Channel 9(1) |
0x38b8 |
14521 |
40 |
– |
– |
|
|
Channel 10(1) |
0x38e0 |
14561 |
40 |
– |
– |
|
|
Channel 11(1) |
0x3908 |
14601 |
40 |
– |
– |
|
|
(1) The detailed information for channels 2 to 11 has the same structure as the detailed information for channel 1. To address the channel N (1≤ N ≤ 11) registers, add 40 × (N – 1) to the channel 1 registers. |
||||||