DOCA0302EN-04

Resetting to Factory Parameters

Description

To reset the I/O Smart Link device to factory settings, press and hold the reset button (R) on the front face of the I/O Smart Link for more than 10 seconds.

NOTE: After performing the factory reset, the device takes 20-30 seconds to resume normal operation.

The reset data is as follows:

  • The communication parameters become: 19 200 Baud, even parity, one stop bit.

  • The operation counters are set to 0.

  • The running hours counters are set to 0.

  • The counter modification dates are set to the value "1 January 2000".

  • The counter pulse weights are set to 10.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?