Acti 9 Devices without Ti24 Interface
Description
Devices that can be connected to the I/O Smart Link are listed in the following table:
|
Designation |
Product Reference |
Description |
|---|---|---|
|
iEM2000T |
A9MEM2000T |
Single-phase energy meter without display |
|
iEM3110 |
A9MEM3110 |
Three-phase energy meter with display |
|
iEM3155 |
A9MEM3155 |
Three-phase energy meter with display |
|
iEM3210 |
A9MEM3210 |
Three-phase energy meter with display |
|
iEM3255 |
A9MEM3255 |
Three-phase energy meter with display |
|
iPRD (Type 2) |
A9L••••1 |
Withdrawable surge arresters with remote indication contact iPRD65r/iPRD40r/iPRD20r/iPRD8r |
|
iPRD 40r PV (Type 2) |
A9L40271 A9L40281 |
Withdrawable surge arresters with remote indication contact |
|
iPRF1 12.5r (Type 1 + Type 2; Type B+C) |
A9L16632 A9L16633 A9L16634 |
Monobloc surge arresters with remote indication contact |
|
PRD1 25r (Type 1 + Type 2) |
16329 16330 16331 16332 |
Withdrawable surge arresters with remote indication contact |
|
PRD1 Master (Type 1) |
16360 16361 16362 16363 |
Withdrawable surge arresters with remote indication contact |
|
iQuick PRD (Type 2) |
A9L16292 A9L16293 A9L16294 A9L16295 A9L16296 A9L16297 A9L16298 A9L16299 A9L16300 |
Withdrawable surge arresters with integrated backup MCB and remote indication contact |
-
The connection of these devices can be done with an A9XCAU06 or A9XCAC01 pre-wired cable: molded connector (at Smart Link end), and with five wires (at device end).
-
When connecting OF/SD indication contacts to I/O Smart Link, use only OF/SD indication contacts with low level.
The table describes the products that need a low level interface relay to connect to I/O Smart Link:
|
Designation |
Description |
|---|---|
|
IH, IHP |
Timer switches with RBN type low level relays or equivalent |
|
IC |
Light sensitive switches with RBN type low level relays or equivalent |
|
TH, THP |
Thermostats with RBN type low level relays or equivalent |
For more information, refer to technical information from www.se.com.