DOCA0302EN-04

Volt-Free Low Level Indication Contact

Overview

A low level type indication contact (NO or NC) can be connected to input I1 or I2 of an I/O Smart Link channel.

NOTE: A single I/O Smart Link channel can take account of two indication contacts, one contact on input I1 and one contact on input I2.

Wiring

An indication contact can be connected with an A9XCAU06 or A9XCAC01 pre-wired cable: molded connector (at I/O Smart Link end), and with the five wires (indication contact end).

NOTE:
  • @updatedD8
    A maximum of one wire can be connected in each Ti24 connector terminal (A9XC2412).

  • Do not connect a wire with cable end in each of the Ti24 connector terminals.

Example of Connection

The OF and SD contacts of a NSX circuit breaker could be directly connected to I/O Smart Link.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?