DOCA0302EN-04

Surge Arresters

Overview

Acti 9 surge arresters can be connected to I/O Smart Link:

  • The remote transfer contact (indication contact: NO) of an Acti 9 surge arrester can be connected to input I1 or I2 of an I/O Smart Link channel.

  • The SD fault-trip indication contact (indication contact: NC) of the circuit breaker associated to an Acti 9 surge arrester can be connected to input I1 or I2 of an I/O Smart Link channel.

NOTE: A single I/O Smart Link channel can take account of two indication contacts, one contact on input I1 and one contact on input I2.

Wiring

An indication contact can be connected with an A9XCAU06 or A9XCAC01 pre-wired cable: molded connector (at I/O Smart Link end), and with the five wires (indication contact end).

The following wiring is dedicated to surge arresters:

  • iPRD (with a commercial reference ending by 1)

  • iPRD DC

  • iQuick PRD

  • iQuick PF (with remote auxiliary)

  • iPRF1 12.5r

  • PRD1 25r and PRD1 35r

  • PRD1 Master

NOTE:
  • @updatedD8
    A maximum of one wire can be connected in each Ti24 connector terminal (A9XC2412).

  • Do not connect a wire with cable end in each of the Ti24 connector terminals.

Examples of Connection

Example: Electrical diagram dedicated to iPRD surge arrester.

(1) Remote transfer contact of iPRD surge arrester: cartridges status

(2) iSD fault-trip indication contact of iC60 or NG125 circuit breaker associated to iPRD surge arrester

Example: Electrical diagram dedicated to the following surge arresters:

  • iQuick PRD

  • iQuick PF (with remote auxiliary)

(1) Remote transfer contact of surge arrester: cartridges status

Example: Electrical diagram dedicated to iPRF1 12.5r surge arresters:

(1) Remote transfer contact of iPRF1 12.5r surge arrester: surge arrester status

(2) iSD fault-trip indication contact of NG125 circuit breaker associated to iPRF1 12.5r surge arrester

Example: Electrical diagram dedicated to the following surge arresters:

  • PRD1 25r and PRD1 35r

  • PRD1 Master

(1) Remote transfer contact of PRD1 25r and PRD1 35r or PRD1 Master surge arrester: cartridges status

(2) iSD fault-trip indication contact of ComPacT NSXm circuit breaker associated to PRD1 25r and PRD1 35r or PRD1 Master surge arrester

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.