Summary of Channels 1 to 11
Status
|
Address |
Register |
No. |
RW |
Type |
Default value |
Svd |
Function code |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x0078 |
121 |
1 |
R |
BITMAP |
0x0000 |
N |
01, 02, 03, 100-4 |
Electrical status on input 1 of all channels(1). |
|
0x0079 |
122 |
1 |
R |
BITMAP |
0x0000 |
N |
01, 02, 03, 100-4 |
Electrical status on input 2 of all channels(1). |
|
(1) With bit assignment:
Each bit gives the electrical level of input 1 and 2:
|
||||||||
Orders
|
Address |
Register |
No. |
RW |
Type |
Default value |
Svd |
Function code |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x0082 |
131 |
1 |
RW |
BITMAP |
0x0000 |
N |
01, 02, 03, 05, 06, 15, 16, 100-4 |
Open order for Acti 9 product(1). |
|
0x0083 |
132 |
1 |
RW |
BITMAP |
0x0000 |
N |
01, 02, 03, 05, 06, 15, 16, 100-4 |
Close order for Acti 9 product(1). |
|
0x0084 |
133 |
1 |
RW |
BITMAP |
0x0000 |
N |
01, 02, 03, 05, 06, 15, 16, 100-4 |
Deactivation order for product not in the Acti 9 range(1). |
|
0x0085 |
134 |
1 |
RW |
BITMAP |
0x0000 |
N |
01, 02, 03, 05, 06, 15, 16, 100-4 |
Activation order for product not in the Acti 9 range(1). |
|
(1) With bit assignment:
|
||||||||
-
Each bit corresponds to either an open or a closed order relative to the register feature (activated when the bit is at 1).
-
Several channels can be controlled at the same time.
-
The I/O Smart Link device resets the bit to state 0 when the order is taken into account (unless no product is connected to the channel).
-
If bits 0 and 1 are set to 1, there is no effect on the system.
Power or Flow Indicators
|
Channels |
|||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|
|
1 |
2 |
3 |
4 |
5 |
6 |
7 |
8 |
9 |
10 |
11 |
|
|
Input I1 |
14001 |
14003 |
14005 |
14007 |
14009 |
14011 |
14013 |
14015 |
14017 |
14019 |
14021 |
|
Input I2 |
14023 |
14025 |
14027 |
14029 |
14031 |
14033 |
14035 |
14037 |
14039 |
14041 |
14043 |
|
Address |
Register |
No. |
RW |
X |
Unit |
Type |
Default value |
Svd |
Function code |
Description |
|---|---|---|---|---|---|---|---|---|---|---|
|
0x36B0 |
14001 |
2 |
R |
X1 |
D |
Float32 |
0 |
N |
03, 100-4 |
Power or flow indicator for channel 1/input 1. |
The characteristics of the power or flow indicators register are as follows:
-
When the impulse counter (the unit depends on the connected device: energy, gas, water, for example) is connected to input 1 or 2 of channel 1, the register contains the flow value. This is calculated as follows:
-
(3600 x pulse weight)/t, t representing the time in seconds between two pulses. The result is expressed for one hour.
-
-
The pulse weight is 10 by default and can be configured by the Modbus command.
Example: This register indicates the active power between the last two pulses if an iEM2000T device is connected to the channel 1/input 1 (Pulse weight = 10 Wh).
This register is reset to 0:
-
After a duration d = 3 x t (t being the time in seconds between the last two pulses), if 3 x t is less than 5 seconds, the duration d equals 5 seconds
-
After 24 hours without a pulse
-
After loss of the 24 Vdc input/output voltage
The accuracy of the power or flow indication is:
-
5% if the pulse frequency is 5 Hertz or less
-
17% if the pulse frequency equals the maximum frequency of 17 Hertz
Consumption Meters
The consumption meters in this Modbus table indicate the consumption from meters connected to each I/O Smart Link channel (1 to 11).
The consumption value (associated with a channel) is obtained by multiplying the number of pulses (received by either Input I1 or Input I2) by the pulse weight.
|
Channels |
|||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|
|
1 |
2 |
3 |
4 |
5 |
6 |
7 |
8 |
9 |
10 |
11 |
|
|
Input I1 |
14051 |
14053 |
14055 |
14057 |
14059 |
14061 |
14063 |
14065 |
14067 |
14069 |
14071 |
|
Input I2 |
14073 |
14075 |
14077 |
14079 |
14081 |
14083 |
14085 |
14087 |
14089 |
14091 |
14093 |
|
Address |
Register |
No. |
RW |
X |
Type |
Default value |
Svd |
Function code |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x36E2 |
14051 |
2 |
R |
X1 |
UINT32 |
0 |
Y |
03, 100-4 |
Consumption meter on channel 1/input I1. |
-
The number of pulses from inputs I1 and I2 of each channel (1 to 11) are available in registers 14212 (channel 1) to 14614 (channel 11). The number of pulses can be preset by writing to the impulse counter register. For more information, see Operation Counters.
-
The pulse weights of inputs I1 and I2 of each channel (1 to 11) are available and can be set in registers 14230 (channel 1) to 14631 (channel 11). The pulse weight is 10 by default. For more information, see Pulse Weight Settings (Meters).
-
The unit of consumption meter values will be same as that of unit of pulse output of the end device.
Operation Counters
|
Channels |
|||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|
|
1 |
2 |
3 |
4 |
5 |
6 |
7 |
8 |
9 |
10 |
11 |
|
|
Input I1 |
14101 |
14103 |
14105 |
14107 |
14109 |
14111 |
14113 |
14115 |
14117 |
14119 |
14121 |
|
Input I2 |
14123 |
14125 |
14127 |
14129 |
14131 |
14133 |
14135 |
14137 |
14139 |
14141 |
14143 |
|
Address |
Register |
No. |
RW |
X |
Type |
Default value |
Svd |
Function code |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x3714 |
14101 |
2 |
RW |
X1 |
UINT32 |
0 |
Y |
03, 16, 100-4 |
Operation counter for channel 1/input 1: changes from state 1 to state 0. |
Running Hour Counters
|
Channels |
|||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|
|
1 |
2 |
3 |
4 |
5 |
6 |
7 |
8 |
9 |
10 |
11 |
|
|
Input I1 |
14145 |
14147 |
14149 |
14151 |
14153 |
14155 |
14157 |
14159 |
14161 |
14163 |
14165 |
|
Address |
Register |
No. |
RW |
X |
Unit |
Type |
Default value |
Svd |
Function code |
Description |
|---|---|---|---|---|---|---|---|---|---|---|
|
0x3740 |
14145 |
2 |
RW |
X1 |
h |
UINT32 |
0 |
Y |
03, 16, 100-4 |
Running hours counter for channel 1/input 1. Counting starts when the input is activated. |