Acti 9 Reflex iC60 Integrated Control Circuit Breaker With Ti24 Interface
Overview
The Acti 9 Reflex iC60 integrated control circuit breaker:
-
Should have a Ti24 interface (with product references A9C6••••).
-
Can allow the device to be controlled via input Y3 of its Ti24 interface.
The Y3 (24 Vdc) input can be controlled by one of the I/O Smart Link channels.
-
Can be used to indicate the state of the control circuit (O/C) and circuit breaker state (auto/OFF).
The Modbus information in the following table is given for an Acti 9 Reflex iC60 integrated control circuit breaker connected to channel 1.
|
Description |
Address(1) |
No. of register(s) |
Type |
Action |
Values and meanings |
|---|---|---|---|---|---|
|
Status |
|||||
|
O/C status: open/closed status |
0x3778 |
1 |
BITMAP |
R |
bit 0 = 0: circuit breaker open bit 0 = 1: circuit breaker closed |
|
auto/OFF status: handle position |
0x3778 |
1 |
BITMAP |
R |
bit 1 = 0: handle in OFF position (device open) bit 1 = 1: handle in upper position: auto |
|
Orders |
|||||
|
Activation of the open order |
0x3779 |
1 |
BITMAP |
RW |
bit 0 = 1: activation of the open order(2) |
|
Activation of the close order |
0x3779 |
1 |
BITMAP |
RW |
bit 1 = 1: activation of the close order(2) |
|
Counters |
|||||
|
Number of circuit breaker open/close cycles |
0x3784 |
2 |
UINT32 |
RW |
– |
|
Number of trippings |
0x3787 |
2 |
UINT32 |
RW |
– |
|
Load running time |
0x3788 |
2 |
UINT32 |
RW |
in hours |
|
(1) To address the channel N (1≤ N ≤ 11) registers, add 40 × (N – 1) to the channel 1 registers. (2) The I/O Smart Link device resets the bit to state 0 when the order is taken into account (unless no product is connected to the channel). If bits 0 and 1 of address 14201 are activated simultaneously, the I/O Smart Link device does nothing. |
|||||